cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube_FW_F4_V1.5.0/Projects/IS42S16400J SDRAM STM32F429I-Discovery/Examples/FMC/FMC_SDRAM/Src/main.c

doreen
Associate II
Posted on April 28, 2015 at 20:37

We are using the same SDRAM on our board as stm32f429i-disco and my question is about

the example code - STM32F429I-Discovery/Examples/FMC/FMC_SDRAM/Src/main.c

where the initialization is only for BANK2, please confirm. 

Has anybody used and can provide the initialization for all

4 banks of IS42S16400J SDRAM ?

stm32f4xx_ll_fmc.h only provides for BANK1 and BANK2:

/** @defgroup FMC_SDRAM_Command_Target FMC SDRAM Command Target

  * @{

  */

&sharpdefine FMC_SDRAM_CMD_TARGET_BANK2            FMC_SDCMR_CTB2

&sharpdefine FMC_SDRAM_CMD_TARGET_BANK1            FMC_SDCMR_CTB1

&sharpdefine FMC_SDRAM_CMD_TARGET_BANK1_2          ((uint32_t)0x00000018)

/**

  * @}

  */

main.c calls the initialization :

static void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram, FMC_SDRAM_CommandTypeDef *Command)

{

  __IO uint32_t tmpmrd =0;

  /* Step 3:  Configure a clock configuration enable command */

  Command->CommandMode              = FMC_SDRAM_CMD_CLK_ENABLE;

  Command->CommandTarget          = FMC_SDRAM_CMD_TARGET_BANK2;

  Command->AutoRefreshNumber      = 1;

  Command->ModeRegisterDefinition = 0;

  1. The 64-Mbit SDRAM is a high speed CMOS, dynamic random-access memory designed to operate in 3.3 V memory systems containing 67,108,864 bits. it is internally configured as a quad-bank DRAM with a synchronous interface. Each 16,777,216-bit bank is organized as 4,096 rows by 256 columns by 16 bits. The 64-Mbit SDRAM includes an AUTO REFRESH MODE, and a power-saving, power-down mode. All signals are registered on the positive edge of the clock signal, CLK.

    The STM32F429ZIT6 MCU reads and writes data at 80 MHz.

#stm32f429i-disco-fmc-is42s16400j
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0