2025-11-25 4:56 AM
Dear all
I have a complex Flash problem. But even with NUCLEO-C092RC Board and the provided FLASH_EraseProgram example I have Flash erase and/or program problems.
I adapted the original provided ST code a litte to get more information of the problem with the on board LED's.
This is the code I changed: (all the rest is 100% original code)
Problem description (with Keil uVision):
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* STM32C0xx HAL library initialization:
- Configure the Flash prefetch
- Systick timer is configured by default as source of time base, but user
can eventually implement his proper time base source (a general purpose
timer for example or other time source), keeping in mind that Time base
duration should be kept 1ms since PPP_TIMEOUT_VALUEs are defined and
handled in milliseconds basis.
- Low Level Initialization
*/
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* Configure the system clock to 48 MHz */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
/* USER CODE BEGIN 2 */
/* Initialize LED1 and LED2 */
BSP_LED_Init(LED1);
BSP_LED_Init(LED2);
#if !defined (GENERATOR_STM32WL3XX)
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
#endif /* ! GENERATOR_STM32WL3XX */
/* Clear OPTVERR bit set on virgin samples */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
/* Erase the user Flash area
(area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/
/* Get the 1st page to erase */
FirstPage = GetPage(FLASH_USER_START_ADDR);
/* Get the number of pages to erase from 1st page */
NbOfPages = GetPage(FLASH_USER_END_ADDR) - FirstPage + 1;
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Page = FirstPage;
EraseInitStruct.NbPages = NbOfPages;
/* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache,
you have to make sure that these data are rewritten before they are accessed during code
execution. If this cannot be done safely, it is recommended to flush the caches by setting the
DCRST and ICRST bits in the FLASH_CR register. */
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK)
{
/*
Error occurred while page erase.
User can add here some code to deal with this error.
PageError will contain the faulty page and then to know the code error on this page,
user can call function 'HAL_FLASH_GetError()'
*/
/* Infinite loop */
while (1)
{
BSP_LED_On(LED1);
HAL_Delay(200);
BSP_LED_Off(LED1);
HAL_Delay(200);
// Error_Handler();
}
}
/* Program the user Flash area word by word
(area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/
Address = FLASH_USER_START_ADDR;
while (Address < FLASH_USER_END_ADDR)
{
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, DATA_64) == HAL_OK)
{
Address = Address + 8; /* increment to next double word*/
}
else
{
/* Error occurred while writing data in Flash memory.
User can add here some code to deal with this error */
while (1)
{
BSP_LED_On(LED1);
HAL_Delay(100);
BSP_LED_Off(LED1);
HAL_Delay(900);
// Error_Handler();
}
}
}
#if !defined (GENERATOR_STM32WL3XX)
/* Lock the Flash to disable the flash control register access (recommended
to protect the FLASH memory against possible unwanted operation) *********/
HAL_FLASH_Lock();
#endif /* ! GENERATOR_STM32WL3XX */
/* Check if the programmed data is OK
MemoryProgramStatus = 0: data programmed correctly
MemoryProgramStatus != 0: number of words not programmed correctly ******/
Address = FLASH_USER_START_ADDR;
MemoryProgramStatus = 0x0;
while (Address < FLASH_USER_END_ADDR)
{
data32 = *(__IO uint32_t *)Address;
if (data32 != DATA_32)
{
MemoryProgramStatus++;
}
Address = Address + 4;
}
BSP_LED_Off(LED1);
BSP_LED_Off(LED2);
/*Check if there is an issue to program data*/
if(MemoryProgramStatus != 0)
{
/* Turn on LED2 when there are errors detected after data programming */
BSP_LED_On(LED2);
}
else
{
/* No error detected. Switch on LED1 */
BSP_LED_On(LED1);
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}Find attached the full project compiled with Keil.
Hope anybody can see same effect. Thank you for any ideas for solving the problems.
By the way I have more or less similar problem with STM32G0B1 CPU.
Franz
2025-11-25 6:38 AM
Hello @franz2
The example FLASH_EraseProgram work correctly on my side.