cancel
Showing results for 
Search instead for 
Did you mean: 

STM3240g-EVM Ethernet Ping issue

M_2
Associate

Hello ST!

I am working on Ethernet driver, I used UDP client example application for one of my application development. But the issue is when i connected lan cable to EVM the status LED's which is defined to indicate lan cable is connected is always OFF. And also i tried to ping through my PC with IP of EVM ethernet but the response is UNREACHABLE.

Expecting your guidance to resolve this issue.

Thanks,

Madhu.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Piranha
Chief II

If PHY LEDs are OFF, then look for MII/RMII, MAC clocks and pin configuration issues. ETH MAC has 3 main clocks which normally must be enabled and one optional for PTP.

Look at User Manual section 2.16.

Romano1
Associate III

Hello I've the same problem but I'm using a different board (EasyMx Pro V7).