cancel
Showing results for 
Search instead for 
Did you mean: 

STM3240g-EVM Ethernet Ping issue

M_2
Associate

Hello ST!

I am working on Ethernet driver, I used UDP client example application for one of my application development. But the issue is when i connected lan cable to EVM the status LED's which is defined to indicate lan cable is connected is always OFF. And also i tried to ping through my PC with IP of EVM ethernet but the response is UNREACHABLE.

Expecting your guidance to resolve this issue.

Thanks,

Madhu.

2 REPLIES 2
Piranha
Chief II

If PHY LEDs are OFF, then look for MII/RMII, MAC clocks and pin configuration issues. ETH MAC has 3 main clocks which normally must be enabled and one optional for PTP.

Look at User Manual section 2.16.

Romano1
Associate III

Hello I've the same problem but I'm using a different board (EasyMx Pro V7).