2012-09-21 6:07 AM
Hi,
I have
10
STM3240G-EVAL to make traing courses.On one board, I have load 2 programs too quikly ones behind the other. I cannot today load any program.
I
work
with STlink2 and µvision4.Have-you any solution to unlock these board.
Thank-you for the help
Yves mevel2012-09-21 6:45 AM
Try setting BOOT0 HIGH when you restart, this will run the system loader instead of broken user code. Erase the part and write a functional application.
If the ST-Link still can't get control you could try an alternate JTAG pod, or use the serial port and the Flash Loader Demonstration program.