cancel
Showing results for 
Search instead for 
Did you mean: 

STM3221G-EVAL ETHERNET

ahmedzizou690
Associate II
Posted on May 31, 2014 at 16:51

I'm a student of University of Tunisia and I'm using IAR Embedded Workbench for ARM, v. 7.10, 32K Kickstart Edition on WIndows 7...

I am

currently

alternating

,

and my

first

project is to

establish communication between

my computer

and

STM3221g-eval

ethernet

connection

.

 

I

focused on creating

blocks

of the function that

will allow

to transform

a file request

by my client

(web

browser)

on appeal from

subroutine.

#!rocketscience
11 REPLIES 11
Posted on June 02, 2014 at 16:50

I don't have your board, you'll need to get a scope out and verify you have the clock signals where you expect them, and the jumpers as required.

Then you want to use your debugger, and understand at what point, and for what reason, the initialization fails. The software in question is designed for your board, be sure to pick the ''STM3221G-EVAL'' as the target.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ahmedzizou690
Associate II
Posted on June 03, 2014 at 16:34

I'm trying to work with ethernet communication and I started with ''

STM32F2x7 In-Application Programming (IAP) over Ethernet ''.

Example works properly but boards must be connected to the ethernet port before that power the board.

If I plug ethernet cable after powered the board I see ethernet led that blink but I'm not able to connect to the board.

'' the network is not connected ''