cancel
Showing results for 
Search instead for 
Did you mean: 

STM3210E-Eval uClinux Problem

mpodany9
Associate
Posted on April 08, 2011 at 12:59

STM3210E-Eval uClinux Problem

2 REPLIES 2
Nickname12657_O
Associate III
Posted on May 17, 2011 at 14:31

Hi Podany,

Can you remove the LCD, and try again.

Let me know if it is ok?

Regards,

STOne.

mpodany9
Associate
Posted on May 17, 2011 at 14:31

Hi STOne,

I removed the LCD and it worked! thx for the hint.

But could you explain why this happens and what to do about it?

I don't need the LCD now, but maybe in the future.

I also tried to get the jffs version of uClinux to run. But when I install the bootloader (kernel_boot_loader.hex) via RS232 and then try to connect via USB like I did with the tiny bootloader, the board doesn't respond (it's not detected as a usb-device).

Is this problem linked to the LCD problem?

Regards,

max