2018-06-05 1:42 AM
Hello,
I'm working on a project that aims to develop a program for compliance with the TS13 149 (
) standard of passenger counting systems for public transit vehicles produced by the company in which I am doing my work. traineeship. The purpose of the project is to introduce network management protocols based on a TCP / IP (Ethernet) link. To do this, the standard requires a service-oriented architecture (SOA) and the following protocols:SOA:the project must meet a service-oriented architecture
FTP: For file transfer
SSH (Secure Shell): To make secure (encrypted) connections between a client and a server and to have control over a remote terminal. HTTP: Used for data triggered by an event mDNS: Simplifies name resolution and enables dynamic scalability and evolution in a local network. TCP: For data transport DHCP: For automatic configuration of IP parameters of a station or machine IP (IPv4, IPv6): For the address space Ethernet: For the linkMy questions are then:
If the STM microcontrollers support all these protocols, our company is committed to carry out this project with this type of microcontrollers
Thank you all
#stm32 Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-06-11 4:59 AM
Hello,
So after doing a lot of research, I came across this document (list of TCP / IP stacks for STM32):
http://www.emcu.eu/wp-content/uploads/2018/03/STM32-ETHERNET-Solutions.pdf
Thank you