2008-07-13 8:06 PM
STM32 System memory boot - 0x7F command.
2011-05-17 3:39 AM
Hello.
I'm trying to develop a host program like FlashLoader.(My-FlashLoader) The work has almost done except one issue. Some STM32 targets are programmed well by My-FlashLoader. But some targets stop and send ''NACK''. The problem is caused by 0x7F packet. I analyzed the FlashLoader's command flow through a serial monitor program. And I found the 0x7F packet difference(send or not). FlashLoader might distinguish the target and send the second 0x7F command or not. Can anyone tell me about the identifier. // Command flow // 0x7F->0x00->0x02->0x02->0x11->0x11 // 0x11->0x11->0x11->0x11->0x11->0x11->0x11->0x11->0x11->0x11->0x11->0x02->0x02->0x01->0x00 // 0x11->0x73->0x7F->0x43->0x43->0x31->0x31->0x11->0x11 Thank you. :) [ This message was edited by: min21c on 14-07-2008 08:40 ]