2018-04-22 11:54 PM
I used ST supply STM32_AN4502_FW_V2.0.2 for SMBus.When test Read Byte command?0x19 can work?but 0x00 can not ACK right,TIMEOUT happen,Why?
#smbus2018-04-23 1:05 PM
What is your hardware? How is it connected? Have you examined the SDA/SCL lines using an oscilloscope?
JW
2018-04-23 7:52 PM
STM32F072RBT as slave, GUI as master. PMBus communication. When use GUI Read Byte (CMD=0x00), After Add_Rd byte have about 25ms delay then STOP, but use GUI Read Byte(CMD=0x19), All OK.
2018-04-24 3:21 PM
Have you examined the SDA/SCL lines using an oscilloscope?
JW
2018-04-24 5:37 PM
GUI? Do I have to read the app note to understand this? Try to paint a picture where I don't have to imagine the context and connectivity.
Perhaps the Slave doesn't understand/support certain things? If you don't understand whats happen inside the machine provide some diagnostic output via a serial or SWV connection, etc.