2014-11-24 6:13 AM
Hi,
I'm using STM32l151rbt6 MCU. But after few days of running the program the internal RTC starts lagging. I'm not doing RTC calibration. Any other possible reasons?Thanks. #stm32 #rtc2014-12-10 6:50 AM
2014-12-10 8:13 AM
I measured LSE via MCO pin. It was 32.75 to 32.89KHz. I think it's fine. What do you say?
I think it should be solid/stable. Your crystal appears to be out of specification, the 9-12pF crystals are not suitable for STM32 designs, you need the 6-7pF ones. ST uses these MC-306 32.7680K-E3:ROHSIs it possible to provide any means of alert when the LSE fails? Fails how. There's no real mechanism to checking if it's not oscillating properly, other than it stops.2014-12-11 3:59 AM
Hi Clive,
Thanks for the suggestion. I have forwarded this to hardware team. I just want to know in what terms this crystal affects the stability of the RTC?2014-12-11 6:16 AM
I would expect it to be off frequency, and stop/start randomly over voltage and temperature, fail to start, or take a long time to start.
2014-12-11 6:24 AM
Okay. Thanks for the info.
2014-12-12 12:05 AM
Hi Clive,
Please let me know the recommended capacitance values of the Loading capacitors.2014-12-12 5:36 AM
For the EPSON part I mentioned ST uses 6.8pF
http://www.st.com/web/en/resource/technical/document/application_note/CD00221665.pdf