cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 RTC Alarm Not configuring

Manjunatha S
Associate II
Posted on June 26, 2014 at 15:07

Hi,

I am using STM32l151vbt6 MCU and I am trying to configure RTC Alarm for ever 15th minute that is 0, 15, 30 and 45th minute of the every hour. I can configure the Alarm and it will work for the first time, If  I try to set it again after the alarm occurs, it would set to previous alarm state. If i reset the MCU i can set the alarm and it will wake the controller from the stop mode when the alarm occurs, Please let me know how can i set the next alarm without resetting the MCU.

Alarm Configure Code:

/*~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~*/

/* 8(hour) and 19(day) are masked and there is no effect on the alarm */

RTC_AlarmTypeDef RTC_AlarmStructure =

{

0,

0,

0,

RTC_H12_AM,

(RTC_AlarmMask_DateWeekDay | RTC_AlarmMask_Hours),

RTC_AlarmDateWeekDaySel_Date,

19

};

const uint32_t alarm_interval[4] = { 15, 30, 45, 0 };

/*~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~*/

RTC_Read();

RTC_AlarmStructure.RTC_AlarmTime.RTC_Minutes = alarm_interval[RTC_current_time.minute / 15];

RTC_Alarm_Config(&RTC_AlarmStructure);

void RTC_Alarm_Config(RTC_AlarmTypeDef *RTC_AlarmStructure)

{

/*~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~*/

EXTI_InitTypeDef EXTI_InitStructure;

NVIC_InitTypeDef NVIC_InitStructure;

/*~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~*/

RTC_AlarmCmd(RTC_Alarm_A, DISABLE);

/* EXTI configuration */

EXTI_ClearITPendingBit(EXTI_Line17);

EXTI_InitStructure.EXTI_Line = EXTI_Line17;

EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;

EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;

EXTI_InitStructure.EXTI_LineCmd = ENABLE;

EXTI_Init(&EXTI_InitStructure);

/* Enable the RTC Alarm Interrupt */

NVIC_InitStructure.NVIC_IRQChannel = RTC_Alarm_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

RTC_SetAlarm(RTC_Format_BIN, RTC_Alarm_A, RTC_AlarmStructure);

/* Clear RTC AlarmA Flags */

RTC_ClearITPendingBit(RTC_IT_ALRA);

/* Enable AlarmA interrupt */

RTC_ITConfig(RTC_IT_ALRA, ENABLE);

/* Enable the alarmA */

RTC_AlarmCmd(RTC_Alarm_A, ENABLE);

}

Alarm ISR:

 EXTI_ClearITPendingBit(EXTI_Line17);

if(RTC_GetITStatus(RTC_IT_ALRA) != RESET)

 {

   /* Clear RTC AlarmA Flags */

            RTC_ClearITPendingBit(RTC_IT_ALRA);

    

 }

#rtc-alarm
2 REPLIES 2
Posted on June 26, 2014 at 17:16

On other STM32 parts I've just advanced the settings in the register.

Perhaps you've not cleared the interrupt/exti properly, but I can't tell from your code.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Manjunatha S
Associate II
Posted on November 24, 2014 at 14:12

Hi Clive,

Thanks for the reply. You can have a look at my code.