2018-01-04 2:25 PM
Just playing with STM32 Primer2 (quite old hardware:
http://www.stm32circle.com/resources/stm32primer2.php
) and have a question related to the debugger interface.This piece of hw uses rlink interface for Ride7 IDE to debug/program the target MCU. The ST72651AR6T1 MCU (32k flash) handles this task (i.e. it steers the SWD pins of the target MCU).
I would like to use the Primer2 with Keil but Keil does not support the rlink (at least I cannot make it use rlink). I wonder if someone solved this problem - ideally I would need st-link firmware for ST72651AR6T1. MAybe there isa another way of solving this problem...
Thanks,
Bogdan
2018-01-04 10:47 PM
Of course I can do some changes on the PCB and connect external programmer but I am looking for less invasive solution...
2018-01-05 12:27 AM
RLink and the
STM32 Primer2
are Raisonance products - so you should contact Raisonance for supporthttp://www.raisonance.com/raisonance-support.html
As Raisonance is a competitor for Keil, it's not surprising that the RLink isn't supported in Keil!
A genuine ST-Link is only ~$20; Chinese imitations are just a couple of dollars.
2018-01-05 3:27 AM
I know, I know, I know...
I purposely mentioned ST7 as it's ST product. Also the target MCU i.e. STMF107 is a ST product. That's why I posted the topic here. I believe it's right place where experienced people share theirs ideas and concerns....
I already mentioned that I can hack the PCB and connect external programmer and looking for an alternative, more subtle way to achieve the same goal.