cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Pinout tables in text or spreadsheet format

ryansturmer2
Associate II
Posted on January 26, 2013 at 22:36

Is there a place that one can get the pinout tables for the STM32 family devices in a format other than PDF?  The tables in the PDF datasheets and reference manuals are not easily copied to other software, and it seems cumbersome and mistake-prone to have to copy the tables by hand into a tool like excel or a text editor.

Particularly, I'm interested in the pinout table for the STM32F0 devices, but if there's a place we can go to get this for any device, that would be awesome.

#pinout-spreadsheet-pdf-textfile
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on January 28, 2013 at 09:32

I have the 'F4xx pinout table reworked into OOo Calc format (which can be converted to Excel or whatever else), as in http://www.efton.sk/STM32/STM32F4xx%20misc.pdf .

There are some xml files available with the MicroXplorer soft, but it may be not trivial to rework them into anything usable.

JW