2025-06-11 7:34 AM - last edited on 2025-06-11 7:47 AM by mƎALLEm
I Tried to flash the uart code in stm32 N657 Nucleo Board, but it is not responding, i was able to make the Leds, blink in the N6 board. Please help me out, i am using the uart example printf code in the N6 stm32 package. I tried the normal method used in the STM32 F4 MCUs, also the selection of peripherals are different in the IOC file. also please explain how to configure the RCC and other peripherals in the IOC file of these N6 boards
Solved! Go to Solution.
2025-08-22 6:21 AM
Hello @VicxSri ;
Is your issue solved or not?
If you need more support please don't hesitate to update post.
If your issue is solved please click on Accept as Solution on the reply which solved your issue.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.