2025-01-02 05:17 PM
Hello First Post, so let me know if I miss anything
Specs:
Stm32WL55JC1 nucleo dev board
waveshare 4.26inch e-Paper display HAT, 800x480, Black/White, SPI Interface
I am Using Stm32WL55JC1 nucleo dev board to develop driver code/application for an epaper display.
my first question is in the example code it does something similar to
#define EPD_4in26_WIDTH 800
#define EPD_4in26_HEIGHT 480
int EPD_test(void)
{
printf("EPD_4in26_test Demo\r\n");
if(DEV_Module_Init()!=0){
return -1;
}
printf("e-Paper Init and Clear...\r\n");
EPD_4in26_Init();
EPD_4in26_Clear();
DEV_Delay_ms(500);
//Create a new image cache
// UBYTE *BlackImage;
/* you have to edit the startup_stm32fxxx.s file and set a big enough heap size */
UDOUBLE Imagesize = ((EPD_4in26_WIDTH % 8 == 0)? (EPD_4in26_WIDTH / 8 :( (EPD_4in26_WIDTH / 8 + 1)) * EPD_4in26_HEIGHT;
UBYTE BlackImage[Imagesize];
printf("Paint_NewImage\r\n");
Paint_NewImage(BlackImage, EPD_4in26_WIDTH, EPD_4in26_HEIGHT, 0, WHITE);
printf("Clear...\r\n");
EPD_4in26_Init();
EPD_4in26_Clear();
printf("Goto Sleep...\r\n");
EPD_4in26_Sleep();
DEV_Delay_ms(2000);//important, at least 2s
// close 5V
printf("close 5V, Module enters 0 power consumption ...\r\n");
DEV_Module_Exit();
return 0;
}
As such it does something similar to this
UDOUBLE Imagesize = (EPD_4in26_WIDTH / 8 )* EPD_4in26_HEIGHT;
we get a value of 48000 or 48k
this is stored in a byte array ie 48kb of storage
why is the width divided by 8?
Second question is my stm32 has 64kb of RAM I assume this is split between the two cores so the core I am programming on has 32KB of ram. is it possible for me to steal ram from the other core and then increase the stack storage to fit in my array or is that impossible?
/*
******************************************************************************
**
** File : LinkerScript.ld
**
** Author : STM32CubeIDE
**
** Abstract : Linker script for STM32WL55xC Device
** 256Kbytes FLASH
** 64Kbytes RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used.
**
** Target : STMicroelectronics STM32
**
** Distribution: The file is distributed as is without any warranty
** of any kind.
**
*****************************************************************************
** @attention
**
** Copyright (c) 2024 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
*****************************************************************************
*/
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 32K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 128K
}
/* Sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
/* The program code and other data into "FLASH" Rom type memory */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH
/* Constant data into "FLASH" Rom type memory */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >FLASH
.ARM.extab (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
{
. = ALIGN(4);
*(.ARM.extab* .gnu.linkonce.armextab.*)
. = ALIGN(4);
} >FLASH
.ARM (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
{
. = ALIGN(4);
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
. = ALIGN(4);
} >FLASH
.preinit_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
{
. = ALIGN(4);
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
. = ALIGN(4);
} >FLASH
.init_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
{
. = ALIGN(4);
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
. = ALIGN(4);
} >FLASH
.fini_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
{
. = ALIGN(4);
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
. = ALIGN(4);
} >FLASH
/* Used by the startup to initialize data */
_sidata = LOADADDR(.data);
/* Initialized data sections into "RAM" Ram type memory */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM AT> FLASH
/* Uninitialized data section into "RAM" Ram type memory */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss section */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM
/* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
} >RAM
/* Remove information from the compiler libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
}
from what I know I can increase Min_stack_size but it does not increase to the size needed to store the array.
Thanks in advance
2025-01-02 08:54 PM
why is the width divided by 8?
Because each epaper pixel can only be black or white. So you only need a single bit to store that information. There are 8 bits in each byte of memory.
I assume this is split between the two cores so the core I am programming on has 32KB of ram
Why do you assume that? Read the Reference Manual for your stm32 and any User Manual for the wireless link you intend to use on the other core. You can choose how much RAM your code accesses on each core. Probably in the “linker script” (I don’t use stm32cube so I don’t know how to do it in that development system).
I don’t like putting large items like the frame buffer onto the stack because there isn’t good protection against stack-overflow. I can see why it would be done as epaper displays aren’t often updated, and it might be useful to use that RAM for other things when not updating the screen. But for simplicity I prefer to have my frame buffer as a static variable.