2017-03-23 7:15 PM
A strange problem occured when i used the STM32_MAT-TARGET to configure the DAC. I configred the DAC output 1 in the STM32F407ZGT6 in cubemx, however, an error always exists shown in the figure. GPIO and ADC are configured and work well. The ioc file is attached. So i am really confused.
2017-03-24 2:16 AM
I have a similar problem.
From my point of view the problem could be that I didn't have the plugin 'Embedded Coder' and so I can not set the path to the STMCubeMx. Maybe the Simulink block has no information about his configuration.
Did you install the 'Embedded Coder' Simulink/Matlab plugin?
So I am really curious for the solution of this problem!
Regards
Stefan
2017-03-24 2:23 AM
Hello,
We will check this case and come back to you.
Could you please precise which version of
STM32_MAT-TARGET
are you using ?Imen
2017-03-24 4:02 AM
STM32-MAT/TARGET version4.4.1
MATLAB version 2016b
Cubemx version 4.20.0
2017-03-24 4:09 AM
I did't install the ''Embedded Coder''. I just follow the hands-on and install the
STM32_MAT-TARGET, as shown in the figure.
Thank you for your answer
Best regards
2017-03-24 4:13 AM
STM32-MAT/TARGET version4.4.1
MATLAB version 2016b
Cubemx version 4.20.0