2010-07-15 6:51 AM
STM32 IWDG Hardware Mode Problem
#freeze #option-file #iwdg #iwdg #problem #stm32 #stm322011-05-17 4:58 AM
I couldn't try this code part because i can't make debug when i enable STM32F10xOPT.s file.
2011-05-17 4:58 AM
Hi,
I use the following code, executed every power-up, to verify that the IWDG is programmed and enabled: /* make sure hardware watchdog is enabled */ option = FLASH_GetUserOptionByte (); if (option & FLASH_OBR_WDG_SW) { FLASH_Unlock (); FLASH_UserOptionByteConfig (OB_IWDG_HW, OB_STOP_RST, OB_STDBY_RST); FLASH_Lock (); } I also use something similar to make sure read-out protection is enabled. Hope that helps.2011-05-17 4:58 AM
I don't know what ''STM32F10xOPT.s'' is. What code does it contain? Why do you need it?
2011-05-17 4:58 AM
This assembly file is the option file of STM32F10x serie. You can select iwdg mode (hw or sw) by this file but it seems i can't enable iwdg module. When i downloading *.hex code, ulink2 programs the option byte area of flash memory and nothing changes in my application.
You can reach detailed information about option file by using the link below. http://www.keil.com/support/docs/3406.htm