cancel
Showing results for 
Search instead for 
Did you mean: 

I2C clock stretching in master mode and other I2C issues

DiBosco
Senior II
Posted on July 15, 2010 at 17:13

I2C clock stretching in master mode and other I2C issues

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
greg_t
Associate II
Posted on May 17, 2011 at 13:58

Hello,

Clock streching is used by slow slaves .. If your slave perform some calculations or other tasks with the recieved data on I2C it holds the clock low until finished proccesing the data (may be interrupt routine ). After releasing the clock the Master may send another byte of data .....

stforum2
Associate II
Posted on May 17, 2011 at 13:58

We found it necessary to reset the I2C (in order to clear the busy bit if I recall):

    g_pRCC->APB1ENR |= I2C1EN;

    g_pI2C1->CR1 = I2C_SWRST;

    g_pI2C1->CR1 = 0;

    g_pI2C1->CCR = I2C_CCR7 | I2C_CCR5;

    g_pI2C1->TRISE = 0X09;

    g_pI2C1->CR2 = I2C_FREQ5;

    g_pI2C1->CR1 = I2C_PE;

DiBosco
Senior II
Posted on May 17, 2011 at 13:58

@Gregory, thanks for the clarification.

@Crossware, thanks for that, I shall implement that for if/when it gets stuck.

I found an error on the layout of the Atmel chip which seems to have helped a lot as well.