2015-05-03 5:31 PM
I found a bug in stm32f4xx_hal_nand.c module, in ''HAL_NAND_Read_Page'' function!
Need to change this line: *(__IO uint8_t *)((uint32_t)(deviceAddress | ADDR_AREA)) = 0x00; to this: *(__IO uint8_t *)((uint32_t)(deviceAddress | CMD_AREA)) = 0x00; I used the K9F1G08U0D flash memory, and I need to send 2 extra address bytes first (column address) So I decided to write my own driver for K9F1G08U0D, based on stm32f4xx_hal_nand.c Unfortunately I copied Read function with that small issue, and I spent 2 nights to figure out the problem :)2019-01-10 12:55 AM
Hi
Does this bug solved?
can you tell me the line number?