2025-08-19 2:25 AM - edited 2025-08-19 2:42 AM
I'm looking for a solution for regarding this simple problem:
This concerns the NemaGFX library for the GPU2D.
Using the latest NeoChromSDK_NEMAP_1.4.17, some functions have been replaced by new ones, in short:
Deprecated New
-----------------------------------------------------------
nema_vg_paint_set_stroke_width nema_vg_stroke_set_width
nema_vg_draw_ring_generic nema_vg_draw_circular_ring (but is not defined?)
We will find this part in the nema_vg.h header file:
nema_vg_draw_ring_generic: This function is deprecated use nema_vg_draw_circular_ring instead.
However, the problem is that nema_vg_draw_circular_ring seems undefined in any of the header files.
I reported the problem as follows:
Good morning Pavan,
This concerns NeoChromSDK_NEMAP_1.4.17
I have updated the libraries to the latest version of NeoChromSDK.
A few functions are deprecated:
Deprecated New
-----------------------------------------------------------
nema_vg_paint_set_stroke_width nema_vg_stroke_set_width
nema_vg_draw_ring_generic nema_vg_draw_circular_ring (not defined?)
The problem is that the new function "nema_vg_draw_circular_ring" does not seem to exist.
I updated the libraries to this latest version of NeoChromSDK.
What did I do wrong?
Kind regards,
Jack.
I think the problem described is truly the simplest in the world.
But the next answer asked for a screenshot!
So I send a screenshot of that particular part of the nema_vg.h header file:
In todays response, a FULL-PAGE screenshot is requested!
That would just add irelevant information only.
I'm sereously disappointed with ST's support regarding this matter, as this doesn't move solutions forward at all, I believe.
Maybe the issue is addressed to the wrong group?
Maybe the issue should be forwarded to someone else?
Is there anybody who can help out?
Best regards,
Jack