2023-02-08 4:19 AM
Hi everyone,
I am trying to send data from one STM32G0B1 MCU to another STM32G0B1 MCU. When i use standard ID it works perfectly but if i use Extended ID then the receiver interrupt doesn't fire.
I also checked it with logic analyzer. Transmitter sending the data but the receiver side is not receiving it. This happens only when i use extended ID.
2023-02-08 5:01 AM
That is weird.
What kind of XTAL are you using in your STM32G0B1's?
2023-02-13 12:56 AM
I am not using any external clock. I am also attaching the transmitter side and receiver side code snippets and also the logic analyzer data.
Transmitter side:
/* Prepare Tx message Header */
TxHeader.Identifier = 0x19800540;
TxHeader.IdType = FDCAN_EXTENDED_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.DataLength = FDCAN_DLC_BYTES_8;
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_ON;
TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData);
HAL_Delay(1000);
}
/* USER CODE END 3 */
}
Receiver Side:
//Configure reception filter to Rx FIFO 0
sFilterConfig.IdType = FDCAN_EXTENDED_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x19800540;
sFilterConfig.FilterID2 = 0x19820540;
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
// Configure global filter:
// Filter all remote frames with STD and EXT ID
// Reject non matching frames with STD ID and EXT ID
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
Error_Handler();
}
// Activate Rx FIFO 0 new message notification
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
{
Error_Handler();
}
void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
if((RxFifo0ITs & FDCAN_IT_RX_FIFO0_NEW_MESSAGE) != 0)
{
//Retrieve Rx messages from RX FIFO0
if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
{
Error_Handler();
}
}
I have connected logic analyzer on Receiver side and it shows the data on RX pin but Receiver FIFO is empty.