cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 DISCOVERY BOARD WITH STM32F10x_StdPeriph_Lib_V3.5.0

jai23
Associate II
Posted on May 19, 2012 at 15:38

I am new to STM32 discovery and using the program  package  STM32F10x_StdPeriph_Lib_V3.5.0. I am trying to run adc module with this package .

But when, I run that code provided into example into STM32 discovery board. Its not working.

I see with debugger that program is stuck at a function Hard_fault_handler();

Please help me in moving to right direction.
4 REPLIES 4
raptorhal2
Lead
Posted on May 19, 2012 at 15:54

More information will improve the quality of the help you get:

Which Discovery board ?

Which IDE ?

Provide code.

Cheers, Hal

Posted on May 19, 2012 at 15:54

Note that there are (at least) four different ''STM32 Discovery'' boards - which one, exactly, are you using?

Have you tried the unmodified examples specifically for your particular board?

Posted on May 19, 2012 at 15:56

Snap!

jlchoobs
Associate II
Posted on June 10, 2012 at 14:32

Don't bother worrying about N's negative comments.

He has been doing this all through the forum.

Some kid who likes crittiquing everybody - without any actually helpful advice.