STM32 CUBE SDIO 4bit problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-11-24 7:19 AM
Posted on November 24, 2014 at 16:19
Hello;
I want to use 4Bit SDIO on STM32F407VGT6 MCU. I already set all parameters on lastest STM32CubeMx software. RCC => External XtallSDIO =>4bit busMy Ide is KEIL 4.73.But this configuration is not working. When i use SDIO 1bit mode , it is works! I already tested my board and connections(pull-ups,caps...) with ''https://github.com/MaJerle/stm32f429/tree/master/21-STM32F429_FATFS'' 4Bit SDIO Example. So my board is working 4bit SDIO mode with this example. I checked with oscilloscope. How can i run 4bit SDIO FATFS with STM32cubemx on STM32F4?Bests,Thanks.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-12-11 5:59 AM
Posted on December 11, 2014 at 14:59
PS: You can refer to the stm324x9i_eval_sd.c/stm324xg_eval_sd.c BSP drivers, that may help you!
Regards,
Heisenberg.
Hi,
The 4-bit SD Data Transfer Mode is Mandatory for High-Speed Cards, Optional for Low-Speed ones, so it depends on the used uSD card type. Otherwise, it's better to configure first the 1-bit SD Data Transfer Mode:hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
And then, just enable wide operation, for the 4-bit SD Data Transfer Mode:
HAL_SD_WideBusOperation_Config(&hsd, SDIO_BUS_WIDE_4B);
Here below some screen captures from the RM0090 reference manual: