cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Cube Problem at generating Code for Nucleo Board F303 RE

gschnittker9
Associate II
Posted on December 01, 2015 at 10:27

Hello,

i try to generate Sourcecode for the Nucleo Board F303 RE with STM32 Cube.

I Use the Toolchain MDK-ARM V5.

At the code-generation I get the following message :

The code is successfully generated under .... but MDK-ARM V5project generation have a problem.

What may be the reason ?

Best regards,

Georg

#keil-mdk-pro-stm32cube #stm32-cube
2 REPLIES 2
Nesrine M_O
Lead II
Posted on December 01, 2015 at 11:23

Hi Georg,

1- If you are using an old version of CUBEMX, I recommend you to use the last version 

2- Is it a recurrent issue or faced only one time?

3- Maybe it is due to lack of space in your disk?

4- Do you face the same issue with another machine?

-Syrine –

gschnittker9
Associate II
Posted on December 01, 2015 at 15:55

1-

The error occurs

also with

the current

Version 4.11

.

Previously I had

the older

version 4.10

installed

.

2 - The error occurs every time I try to generate code.

3 -

The

space on the

hard disk is

not

too big, but

is

still

70GB

free

.

4 - Now I tried it on an other machine, and it works.

The other machine

is

at least

a

workaround.

Thanks !