2023-11-25 4:34 AM
hi there,
I want to communicate between two Stm32 using SPI, when i transmit date from master to slave, it received(using received interrupt). but when want to transmit date from slave side it gives HAL_error,
master side code
while (1)
{
for(int i=0; i<9;i++)
{
HAL_GPIO_WritePin(SPI1_NSS_GPIO_Port, SPI1_NSS_Pin, GPIO_PIN_RESET);
// HAL_Delay(10);
HAL_UART_Transmit (&huart1, "OK1\r\n", 5, 10);
data[0] = 0x40 + i; // multibyte write
data[1] = 0x60 ;
status = HAL_SPI_Transmit (&hspi1, data, 2, 1000); // write data to register
// HAL_Delay(10);
status = HAL_SPI_Receive (&hspi1, Rxdata, 2, 5000); // write data to register
HAL_GPIO_WritePin(SPI1_NSS_GPIO_Port, SPI1_NSS_Pin, GPIO_PIN_SET);
if(Rxdata[0] == 0x11)
{
HAL_UART_Transmit (&huart1, "Received11\r\n", 12, 10);
}
HAL_Delay(1000);
}
Slave side code
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
HAL_SPI_Receive(&hspi1, data, 2, 5000); // write data to register
Spi_rcvr_flag= 1 ;
}
whenever the CS goes to low state, slave become ready to receive the data.
while(hspi1.State != HAL_SPI_STATE_READY);
if(Spi_rcvr_flag){
if(data[1] == 0x60 && data[0] == 0x40 )
{
status = HAL_SPI_Transmit (&hspi1, (uint8_t)*TXdata, 2, 5000);
while(hspi1.State != HAL_SPI_STATE_READY);
if(status == HAL_OK){
HAL_UART_Transmit (&huart1, "Received 0\r\n", 13, 10);}
}
else if(data[1] == 0x60 && data[0] == 0x41 )
{
HAL_SPI_Transmit (&hspi1, TXdata, 2, 1000);
HAL_UART_Transmit (&huart1, "Received 1\r\n", 13, 10);
}
else if(data[1] == 0x60 && data[0] == 0x42 )
{
HAL_SPI_Transmit (&hspi1, TXdata, 2, 1000);
HAL_UART_Transmit (&huart1, "Received 2\r\n", 13, 10);
}
else if(data[1] == 0x60 && data[0] == 0x43 )
{
HAL_SPI_Transmit (&hspi1, TXdata, 2, 1000);
HAL_UART_Transmit (&huart1, "Received 3\r\n", 13, 10);
}
else if(data[1] == 0x60 && data[0] == 0x44 )
{
HAL_SPI_Transmit (&hspi1, TXdata, 2, 1000);
HAL_UART_Transmit (&huart1, "Received 4\r\n", 13, 10);
}
else if(data[1] == 0x60 && data[0] == 0x45 )
{
HAL_SPI_Transmit (&hspi1, TXdata, 2, 1000);
HAL_UART_Transmit (&huart1, "Received 5\r\n", 13, 10);
}
else if(data[1] == 0x60 && data[0] == 0x46 )
{
HAL_SPI_Transmit (&hspi1, TXdata, 2, 1000);
HAL_UART_Transmit (&huart1, "Received 6\r\n", 13, 10);
}
else if(data[1] == 0x60 && data[0] == 0x47 )
{
HAL_SPI_Transmit (&hspi1, TXdata, 2, 1000);
HAL_UART_Transmit (&huart1, "Received 7\r\n", 13, 10);
}
else if(data[1] == 0x60 && data[0] == 0x48 )
{
status = HAL_SPI_Transmit (&hspi1, TXdata, 2, 5000);
if(status == HAL_OK){
HAL_UART_Transmit (&huart1, "Received 8\r\n", 13, 10);}
}
else if(data[1] == 0x60 && data[0] == 0x49 )
{
HAL_SPI_Transmit (&hspi1, TXdata, 2, 1000);
HAL_UART_Transmit (&huart1, "Received 9\r\n", 13, 10);
}
Spi_rcvr_flag= 0 ;
}
but at the receiver side it HAl_Error and in master side both byte recievd same data.
please guide how to make SPI slave library,
thanking you
2023-11-25 5:36 AM
as I am transmitting 0x11 and 0x22 data from slave side with HAL_error.
then master side i received 0x22 and 0x22 in both pck byte.
2023-11-30 5:01 AM
now after number of try and error method I am able to transmit 16 byte s of data,
why this happened I am not going to understands,
please guide some one guide me who already gone through this problem or have done this communication,
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
if(!HAL_GPIO_ReadPin (GPIOG, GPIO_PIN_10)){
HAL_SPI_Receive(&hspi1, data, 98, 1000); // write data to register
while(hspi1.State != HAL_SPI_STATE_READY);
//HAL_SPI_Transmit (&hspi1, (uint8_t)*TXdata, 2, 5000);
Spi_rcvr_flag= 1 ;
}
if(HAL_GPIO_ReadPin (GPIOG, GPIO_PIN_10))
{
// while(hspi1.State != HAL_SPI_STATE_READY);
HAL_SPI_Transmit (&hspi1, &TXdata, 16, 1000);
while(hspi1.State != HAL_SPI_STATE_READY);
}
Thanking You,
Yogesh Nandurkar