cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 and external (S)DRAM

Posted on April 13, 2011 at 11:29

STM32 and external (S)DRAM

3 REPLIES 3
trevor23
Associate III
Posted on May 17, 2011 at 14:31

Can't be DRAM, must be SRAM. You can get 8M (4M x 16) e.g. CY62187EV30.

This seems an ambitious project for a microcontroller such as the STM32 which isn't really that suited to running code from external memory.

Posted on May 17, 2011 at 14:31

Thank you for the info about the SRAM module.

Why is the STM32 not suited to running code from external memory?

Do you see other options to run code from a SD-Card (or maybe an other Cortex-M3 microcontroller which is better suited for such thing)?

Greets

Christoph

Posted on May 17, 2011 at 14:31

Because external bus access is relatively slow, and the part doesn't have a cache.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..