cancel
Showing results for 
Search instead for 
Did you mean: 

STM Virtual COM Port + Windows 8

toinetteleed
Associate II
Posted on December 11, 2013 at 13:57

Is it possible to install/use the STM Virtual COM Port on Windows 8? 

#windows-8
3 REPLIES 3
Posted on December 11, 2013 at 17:29

Probably, if the driver is unsigned you'll need to turn off that test for it to load/work.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
toinetteleed
Associate II
Posted on December 13, 2013 at 10:55

I tried turning off the signed driver protection. It didn't help. I have also tried running the driver in compatibility mode and as administrator. No luck.

toinetteleed
Associate II
Posted on January 27, 2014 at 07:51

Good news: I upgraded the Windows 8 computer to Windows 8.1 and the STM Virtual COM Port now successfully installs and works. It is not ideal that I cannot use Windows 8 without the upgrade, but it is still great that the driver does work on a version of the newer OS.