cancel
Showing results for 
Search instead for 
Did you mean: 

STM Virtual Com port win11 driver needed

StanJerm
Associate III

hello, where can i download win11 STM virtual com port?  i install both VCP_V1.5.0_Setup_w7_x64_64bits and W8_x86_32bit all not working ! i din see

STM Virtual Com port at device manager! only STM STLink visual com port appear ... 

12 REPLIES 12

yes.. i hav a program but seems its not working,,,

Yaswanthi
Associate

 I am facing similar issue , STM Virtual Com port not appearing at device manager when I  plug usb cable . Were you able to resolve this?

RalfV
Associate

Having similar issues with the EVL6482H-Discovery board, latest firmware flashed shows up as a HID compliant barcode reader under windows 11.

HID\VID_0483&PID_7004&REV_0110
HID\VID_0483&PID_7004
HID\VID_0483&UP:008C_U:0001
HID_DEVICE_UP:008C_U:0001

It identifies as a HID compliant device with 2 endpoints