2014-01-15 1:55 PM
Im using STM Studio 3.3.
When I import my .elf files from Keil or Coocox most of the variables (even direct variables) are missing. When I analyze the .elf file with nm or eu-nm all the variables are available on fix RAM-adresses and I can manually add these adresses to the read or write list. What is wrong with importing the .elf files in STM Studio ? #stm-studio2014-01-24 2:51 AM
Hi Henry,
Would it be possible to attach your .elf file for check? What are types of missing variables? -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.