Skip to main content
waclawek.jan
Super User
February 22, 2017
Question

STLink: How to hold target under reset?

  • February 22, 2017
  • 6 replies
  • 3906 views
Posted on February 22, 2017 at 15:16

How can I *hold* target connected to STLink under reset, either using CLI or GUI version of STLinkUtility, or any other software tool?

ST: If there's no provision for this in STLink Utility, then please consider this as a feature request.

Thanks,

Jan Waclawek

    This topic has been closed for replies.

    6 replies

    Nesrine M_O
    Associate
    February 22, 2017
    Posted on February 22, 2017 at 16:32

    Hi

    Waclawek.Jan

    ,

    The “connect under reset�? option is available with ST-LINK/V2, it

    allows to connect to the target before executing any instruction:

    • STM32 ST-LINK utility

      GUI version

    0690X00000606NjQAI.png

    • STM32 ST-LINK utility command line interface (CLI)

      :

      [UR]: Connect to the target under reset

      .

    It seems this is not what you are looking for, so:

    1. Could you please precise the purpose of such request?
    2. what kind of application case leads to this request?

    -Nesrine-

    waclawek.jan
    Super User
    February 22, 2017
    Posted on February 22, 2017 at 17:31

    Nesrine,

    Thanks for your reply.

    I am aware of the 'Connect Under Reset option'. This is not what I am looking for - when used, NRST output of STLink goes down during the connection phase, but the the debugger puts the core into halt and releases the NRST line, so the resulting behaviour is a short pulse.

    Simply put, I'd like to have a tickbox (or command for CLI) which directly sets and/or releases the NRST output of STLink.

    Rationale:

    In larger systems, the mcu reset is connected to reset inputs of other chips. During debugging, sometimes it is needed to hold the whole system in reset. Once this line is connected to STLink, it would be an added bonus if it could be directly manipulated from PC.

    Thanks.

    Jan

    Nesrine M_O
    Associate
    February 27, 2017
    Posted on February 27, 2017 at 11:15

    Hi

    Waclawek.Jan

    ,

    I forward your request to our team,I will come back when i have more information.

    Thank you very much for your contribution to the enhancement of our STM32 related solutions.

    -Nesrine-

    Paul Wearne
    Associate
    March 14, 2017
    Posted on March 14, 2017 at 23:04

    I would like to use the ST-Link Utility CLI, as part of my high-level software test environment. I would like the ability to hold the microprocessor in reset, while the high level test test environment is setup to stimulate and monitor the software build under test.