Stepper motor, timer phase control
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-07 2:26 PM
Posted on August 07, 2014 at 23:26
I am setting up stepper motor control on an STM32F4xxx using Full Step Drive as in http://en.wikipedia.org/wiki/File:Drive.png
Both timers are setup as up counters with PWM output. Timer 2 controls phases A & C. Timer 5 controls phases B & D. Example with fixed frequency:TIMER 2CNT = 4000CCR1 = 2000 (CNT/2)CCR2 = 2000 (with complement output)CCR3 = 1000 (CNT/4)TIMER 5CNT = 4000CCR3 = 2000CCR4 = 2000 (with complement output)GPIO setup to output on PA0..PA3I need something like timer 2 CCR3 rising edge to reset timer 5. Specifically to reset timer 5 counter to zero and to load CNT, CCR3 and CCR4 from their shadow registers.The stepper motor must have a variable speed. For speed changes timer 2 interrupts on counter reload. In the ISR its CNT, CCR1, CCR2 and CCR3 are changed unbuffered. (No change is more than 2%.) At the same time timer 5�s CNT, CCR3 and CCR4 registers are changed to go into effect when timer 2 triggers reset via ITR0 (TRGO from CCR3).At least that�s how it�s supposed to work.However, docs are fuzzy about the various settings to make all this work. I likely have most of it:TIMER 2 (master)CR1 = 1 (simple on, unbuffered, up count etc)CR2 MMS = 110b (OC3REF signal is used as trigger output -- TRGO)SMCR top 8 bits all zero TS = 000b (is this important for ITR0?) SMS = 000b (Does this means timer 2 is the master?)CCMR2 OC3CE = 0 OC3M = 110b (standard positive PWM output) OC3PE = 0 (new CCR3 takes effect immediately - also OC1PE & OC2PE) OC3FE = 0 (is this bit irreverent here?) CC3S = 00b (output mode)TIMER 5 (slave)CR1 = 0x85 (on, buffered, ) APPE = 1 (buffered ARR) URS = 1 (What does this do? Anything?) CEN = 1 enable counterCR2 MMS = 000b (what�s the value most likely to be ignored?)SMCR top 8 bits all zero MSM = 0 TS = 000b (use internal trigger ITR0) SMS = 100b (trigger forces slave to act like counter hit max??)CCMR2 MSM = 0 (x=3 and 4) OCxCE = 0 (whatever does this do?) OC3M = 110b OC4M = 111b OCxPE = 0 (is this correct for buffered?) OCxFE = 0 (is this correct for buffered?) CCxS = 00b (output mode)Yet when the millisecond timer takes my OS out of WFI both CNT registers are equal. What don�t I understand? #stepper-motor #timer-phase
Labels:
- Labels:
-
TIM
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-07 4:34 PM
Posted on August 08, 2014 at 01:34
For phase relative control from a single timer consider using toggle mode, and advancing\retarding CCRx points to control edge/phase placement.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-07 5:48 PM
Posted on August 08, 2014 at 02:48
Good thought. Thanks. Toggle phases A & C using CCR1=CCR2=1. Toggle phases B & D using CCR3=CCR4=(CNT/2)+1. And that only uses one timer!
But can I set starting outputs on PA0..3 by setting GPIOA_BSRR to 0x000A0005? Or is the start point for toggles contained within the timer? Setting BSRR is a piece of cake. Finding something hidden within the timer could be a problem..Assuming BSRR works (fingers crossed) reverse (after stopping the timer) is likely a simple BSRR=0x00060009. Will try sometime next week using a logic analyzer.