2017-03-02 11:43 AM
Hi,
I'm using the Waveshare Open746I-C Package B based on the STM32F746 development board with StemWin with 2 Meg SDRAM, on FreeRTOS, GT811 touch screen interface and 7 inches 1024x600 LCD.
After many hours of debugging everything works fine but I’m still facing a strange issue. Doing a simple two buttons GUI, the board goes directly into goes directly into my HardFault_Handler manager if the Framewin_CreateIndirect first coordinates are 0, 0.
staticconst
GUI_WIDGET_CREATE_INFO
_aDialogCreate
[] = { {
FRAMEWIN_CreateIndirect
,'Framewin'
,ID_FRAMEWIN_0
, 0, 0, 1024, 600, 0, 0x0, 0 }, {BUTTON_CreateIndirect
,'Test 1'
,ID_BUTTON_0
, 818, 390, 150, 67, 0, 0x0, 0 }, {BUTTON_CreateIndirect
,'Test 2'
,ID_BUTTON_1
, 818, 470, 150, 67, 0, 0x0, 0 },// USER START (Optionally insert additional widgets) // USER END };
But if the Framewin starts another value like -1, 0 or 1, 0 than everything works fine, can someone with STemWin experience could tell me what I'm doing wrong?
staticconst
GUI_WIDGET_CREATE_INFO
_aDialogCreate
[] = { {FRAMEWIN_CreateIndirect
,'Framewin'
,ID_FRAMEWIN_0
, -1, 0, 1024, 600, 0, 0x0, 0 },Regards.
2024-03-17 6:27 AM
Hi,
This might be outside ur issue. but i've also purchased same kit. but couldnt bring up display.
basically i couldnt use the sample code waveshare provided for 7inch display to be compatible with stm32 cube ide.
can u pls help me with sample code if any?
Anand.