2013-09-03 1:47 AM
Hello everybody,
I would like to try STemWIN library with CoIDE environment. I check that the examples only for the payed license tools. I try set up the CoiDE project but I've linker errors. [cc] c:/program files (x86)/gnu tools arm embedded/4.7 2012q4/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: lcd_teszt.elf section `.ExtRAMData' will not fit in region `ram' [cc] c:/program files (x86)/gnu tools arm embedded/4.7 2012q4/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: region `ram' overflowed by 403488 bytes [cc] ..\..\..\..\..\..\..\Users\tjo2bp\Downloads\STemWin_Library_V1.0.0\Libraries\STemWinLibrary520d\Lib\libstemwin520d_cm4_gcc.a(WM_Motion.o): In function `_AimDestinationXY': [cc] WM_Motion.c:(.text._AimDestinationXY+0x6e): undefined reference to `sqrt' [cc] ..\..\..\..\..\..\..\Users\tjo2bp\Downloads\STemWin_Library_V1.0.0\Libraries\STemWinLibrary520d\Lib\libstemwin520d_cm4_gcc.a(WM_Motion.o): In function `_MoveToNearestSnapPositionXY': [cc] WM_Motion.c:(.text._MoveToNearestSnapPositionXY+0x6a): undefined reference to `sqrt' [cc] GUIDEV_Perspective.c:(.text.GUI_MEMDEV_DrawPerspectiveX+0x168): undefined reference to `sqrt' [cc] ..\..\..\..\..\..\..\Users\tjo2bp\Downloads\STemWin_Library_V1.0.0\Libraries\STemWinLibrary520d\Lib\libstemwin520d_cm4_gcc.a(GUI_Valf.o): In function `_RoundHalfUp': [cc] GUIDEV_Perspective.c:(.text.GUI_MEMDEV_DrawPerspectiveX+0x13c): undefined reference to `sqrt' [cc] GUI_Valf.c:(.text._RoundHalfUp+0x20): undefined reference to `ceil' [cc] ..\..\..\..\..\..\..\Users\tjo2bp\Downloads\STemWin_Library_V1.0.0\Libraries\STemWinLibrary520d\Lib\libstemwin520d_cm4_gcc.a(GUIDEV_Perspective.o): In function `GUI_MEMDEV_DrawPerspectiveX': [cc] GUI_Valf.c:(.text._RoundHalfUp+0x36): undefined reference to `floor Is anyone has a working project with CoIDE? Thanks2013-11-09 9:18 AM
Hello toth.janos
Have you succeeded with STemWIN + CooCox CoIDE? May I have a copy of your example project folder? I may be contacted: gordonkevin117(at)gmail.com
Many thanks, Kevin2013-11-09 9:58 AM
At least two things going on there. First the absence of a floating point support library, and secondly with the linker script and the placement of data in the external RAM. You'd want to check the size allocated to various memory regions, and how those regions are initialized. Any data placed in RAM (statics) has to also be placed in flash and copied to RAM by the C runtime library during start up. If initialized data is too big to fit in either memory, you might need to rethink the strategy. ie Loading bitmaps, etc, from storage media.
I, personally, am not going to wade into the hot mess that is CooCox, I might be convinced to demonstrate compilation under GNU/GCC with Yagarto.2013-11-12 9:16 PM
Hello Clive1,
I am interested in your comments. I visited
because I want to find the best system for me. The author of the page seems to try anything to encourage the visitor to move elsewhere. What is your opinion regarding emIDE? Next the writer sends the visitor tohttps://launchpad.net/gcc-arm-embedded
which is the same toolchain used by coocox.org. Then he thanks the visitor for listening and sends them to which has a front page that states: ?Permanently under construction :o)?. Finally at the bottom of the yagarto page comes the link to:http://sourceforge.net/projects/yagarto/
where the toolchain was last updated 22 Dec 2012. I then visited where deep in the archive I found ?GNU ARM Bare Metal Toolchain?, no mention of yagarto in the summary. Thank goodness on the page itselfhttp://www.emb4fun.de/archive/gabmt/index.html
the writer begins the installation. But? another attempt to divert the visitor tohttps://launchpad.net/gcc-arm-embedded
. However I continued down the page and installed the tools and yagarto then compiled the test example. Success! Finally for support the writer sent the visitor tohttp://embdev.net/forum/arm-gcc
which is a plus! But I then realised at the top of the pagehttp://www.emb4fun.de/archive/gabmt/index.html
I had missed steps 1 and 3. Now I am on another archive pagehttp://www.emb4fun.de/archive/gdbserver/index.html
GDB Server which states that I need J-Link EDUhttp://www.segger.com/cms/j-link-edu.html
to be able to proceed. In five days it will be delivered.I am a little concerned that at ever step of the way the above sites tried to push me to the compiler/linker used by Coocox.org. I am definitely a beginner needing your help.
I have successfully compiled and linked my stemWin project: Note that in coIDE I have set the compiler settings for FPU to ?FPU Hard?:
GCC HOME: C:\CooCox\GNU Tools ARM Embedded\4.7 2013q3\bin
compile:
[mkdir] Created dir: C:\CooCox\CoIDE\workspace\emWinExample1\emwinexample1\Debug\bin
[mkdir] Created dir: C:\CooCox\CoIDE\workspace\emWinExample1\emwinexample1\Debug\obj
[cc] 8 total files to be compiled.
[cc] arm-none-eabi-gcc -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wall -ffunction-sections -g -O0 -c -DSTM32F407VG -DSTM32F4XX -DUSE_STDPERIPH_DRIVER -D__ASSEMBLY__ -D__FPU_USED -IC:\CooCox\CoIDE\workspace\emWinExample1\cmsis_boot -IC:\CooCox\CoIDE\workspace\emWinExample1\cmsis_lib -IC:\CooCox\CoIDE\workspace\emWinExample1 -IC:\CooCox\CoIDE\workspace -IC:\CooCox\CoIDE\workspace\emWinExample1\inc -IC:\CooCox\CoIDE\workspace\emWinExample1\cmsis -IC:\CooCox\CoIDE\workspace\emWinExample1\cmsis_lib\include -IC:\CooCox\CoIDE -IC:\CooCox\CoIDE\workspace\emWinExample1\Common C:\CooCox\CoIDE\workspace\emWinExample1\GUIConf.c C:\CooCox\CoIDE\workspace\emWinExample1\LCDConf.c C:\CooCox\CoIDE\workspace\emWinExample1\cmsis_boot\startup\startup_stm32f4xx.c C:\CooCox\CoIDE\workspace\emWinExample1\main.c C:\CooCox\CoIDE\workspace\emWinExample1\cmsis_lib\source\stm32f4xx_rcc.c C:\CooCox\CoIDE\workspace\emWinExample1\cmsis_lib\source\stm32f4xx_gpio.c C:\CooCox\CoIDE\workspace\emWinExample1\cmsis_boot\system_stm32f4xx.c C:\CooCox\CoIDE\workspace\emWinExample1\GUI_X.c
[cc] Starting link
[cc] arm-none-eabi-gcc -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wall -g -nostartfiles -Wl,-Map=emWinExample1.map -O0 -Wl,--gc-sections -LC:\CooCox\CoIDE\configuration\ProgramData\emWinExample1 -Wl,-TC:\CooCox\CoIDE\configuration\ProgramData\emWinExample1/arm-gcc-link.ld -g -o emWinExample1.elf ..\obj\GUIConf.o ..\obj\LCDConf.o ..\obj\startup_stm32f4xx.o ..\obj\main.o ..\obj\stm32f4xx_rcc.o ..\obj\stm32f4xx_gpio.o ..\obj\system_stm32f4xx.o ..\obj\GUI_X.o -L..\..\.. -lstemwin522_cm4_gcc
Program Size:
text data bss dec hex filename
31196 20 68204 99420 1845c emWinExample1.elf
BUILD SUCCESSFUL
Total time: 3 seconds
I have five excellent new books on embedded systems. However at this time I am ignorant about memory. ?
the linker script and the placement of data in the external RAM? The word ?external? has caused my 72 year old brain to sunder. I am using a ST32F407VG discovery board (only) with a DM-LCD35RT screen with a display controller SSD2119 (standard add-on to embest base board). I do not have a arm-gcc-link.ld file as I have:
That is about it. The main.c is a small string example for testing. To complete here is one of the greatest marketing spins of all time:
?This library is a professional graphical stack library, enabling the building up of Graphical User Interfaces (GUIs) with any STM32, any LCD/TFT display and any LCD/TFT controller, taking advantage of STM32 hardware accelerations whenever possible.?
Just a little smile while thinking of the modern world.
Many thanks,
Kevin.
2013-11-12 11:36 PM
Your post deserves a long response, but it's the middle of the night here, so I'll keep it brief and come back later.
I've found GNU/GCC 4.7.2 quite serviceable for building apps on the STM32F429I-DISCO and prior boards, along with the 4.6.x before it. I'm using the command line with MAKE for both STM32 M3/M4 targets, and ATMEL ARM9 ones. The compiler, although perhaps a year old is pretty agnostic to the target chip (has intrinsic support for M3 and M4 going way back), something the IDE's seem to have keep iterating around to build templates and configurations for. CodeSourcery/Mentor has some newer builds I'm sure, but they had nag screens, and their own MAKE. I'd use Eclipse with them, and then swapped out the tool chain for the Yagarto ones. This is the USB VCP example I put together for the STM32F429I-DISCOhttps://drive.google.com/file/d/0B7OY5pub_GfIYjU3QTJtWVFHNE0/edit?usp=sharing
2013-11-14 12:49 AM
Hello clive1. Thank you for your reply. I am most interested in the stm32f429i-disco but no supplies in nz until next year (76 days!). I look forward to your reply.
Regards, Kevin2014-01-31 1:34 AM
Hi,
I have the same problem. When i compile, compiler show me this error:C:\TechKnow\STemWin_GUI_lib\STemWin_Library_V1.1.1\Libraries\STemWinLibrary522\Lib\libSTemWin522_CM4_GCC.a(WM_Motion.o): In function `_AimDestinationXY':WM_Motion.c:(.text._AimDestinationXY+0x6e): undefined reference to `sqrt'C:\TechKnow\STemWin_GUI_lib\STemWin_Library_V1.1.1\Libraries\STemWinLibrary522\Lib\libSTemWin522_CM4_GCC.a(WM_Motion.o): In function `_MoveToNearestSnapPositionXY':WM_Motion.c:(.text._MoveToNearestSnapPositionXY+0x6a): undefined reference to `sqrt'collect2.exe: error: ld returned 1 exit statusI have this error only when i use function of WM_MOTION like WM_MOTION_Enable().I've already link the STemWin library and DSP_Lib libarm_cortexM4lf_math.a and set fpu to hard but not change.I try to include <math.h> but the resutl is the same.I use Eclipse Kepler with GCC ARM 4.8 on STM42F429discoveryThaks.Lorenzo
2014-01-31 2:02 AM
I try to include <math.h> but the resutl is the same.
No wonder, your errors are linking errors.I'm not experienced with Coocox, but you need to add ''-lm'' to the linker flags, to actually link in the math library.Problems with the FPU and soft/hard might appear later, but this is not yet the case ...
2014-01-31 2:27 AM
Thanks for fast reply.
I'm not using coocox ide, im using Eclipse + ARM GCCI add ''-lm'' to linker but nothing change.arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -ffunction-sections -fdata-sections -Wall -g -T ''C:/Users/Laboratorio/Eclipse_Workspace/SDC_p1.0.0\\STM32F429ZI_FLASH.ld'' -Xlinker --gc-sections ''-LC:\\TechKnow\\STM32F4_library\\STM32F429I-Discovery_FW_V1.0.1\\Libraries\\CMSIS\\Lib\\GCC'' ''-LC:\\TechKnow\\STemWin_GUI_lib\\STemWin_Library_V1.1.1\\Libraries\\STemWinLibrary522\\Lib'' -Wl,-Map,SDC_p1.0.0.map -lm -o SDC_p1.0.0.elf ''[...](all file compile)C:\TechKnow\STemWin_GUI_lib\STemWin_Library_V1.1.1\Libraries\STemWinLibrary522\Lib\libSTemWin522_CM4_GCC.a(WM_Motion.o): In function `_AimDestinationXY':WM_Motion.c:(.text._AimDestinationXY+0x6e): undefined reference to `sqrt'C:\TechKnow\STemWin_GUI_lib\STemWin_Library_V1.1.1\Libraries\STemWinLibrary522\Lib\libSTemWin522_CM4_GCC.a(WM_Motion.o): In function `_MoveToNearestSnapPositionXY':WM_Motion.c:(.text._MoveToNearestSnapPositionXY+0x6a): undefined reference to `sqrt'collect2.exe: error: ld returned 1 exit statusIt can be a linker script problem? I use the .ld file there is in the STM32F429discovery example and a found section: /* Remove information from the standard libraries */ /DISCARD/ : { libc.a ( * ) libm.a ( * ) libgcc.a ( * ) }If i compile with this the error is:c:/devtools/appli/gnu_arm/bin/../lib/gcc/arm-none-eabi/4.8.3/../../../../arm-none-eabi/lib/armv7e-m/fpu\libm.a(lib_a-w_sqrt.o): In function `sqrt':w_sqrt.c:(.text.sqrt+0x9e): undefined reference to `__errno'w_sqrt.c:(.text.sqrt+0xa8): undefined reference to `__errno'collect2.exe: error: ld returned 1 exit statusif i delete libm.a ( * ) the error isC:\TechKnow\STemWin_GUI_lib\STemWin_Library_V1.1.1\Libraries\STemWinLibrary522\Lib\libSTemWin522_CM4_GCC.a(WM_Motion.o): In function `_AimDestinationXY':WM_Motion.c:(.text._AimDestinationXY+0x6e): undefined reference to `sqrt'C:\TechKnow\STemWin_GUI_lib\STemWin_Library_V1.1.1\Libraries\STemWinLibrary522\Lib\libSTemWin522_CM4_GCC.a(WM_Motion.o): In function `_MoveToNearestSnapPositionXY':WM_Motion.c:(.text._MoveToNearestSnapPositionXY+0x6a): undefined reference to `sqrt'collect2.exe: error: ld returned 1 exit status2014-01-31 4:24 AM
I'm not using coocox ide, im using Eclipse + ARM GCC
I guess I mixed this up with the previous poster ...c:/devtools/appli/gnu_arm/bin/../lib/gcc/arm-none-eabi/4.8.3/../../../../arm-none-eabi/lib/armv7e-m/fpu\libm.a(lib_a-w_sqrt.o): In function `sqrt':
w_sqrt.c:(.text.sqrt+0x9e): undefined reference to `__errno'
w_sqrt.c:(.text.sqrt+0xa8): undefined reference to `__errno'
collect2.exe: error: ld returned 1 exit statusLooks like a library problem.Admittedly I don't have much experience with your toolchain combination.But ''
undefined reference to __errno
'' makes me think you linking against the wrong library, or miss something.The variable ''errno
'' is a common way for several clib functions to return specific errors to the caller. Usually, it is defined in the header ''errno.h'' as ''extern int errno
''.Perhaps including ''errno.h
'' solves your problem.PS: freaking forum software ... !!!!