Posted on April 01, 2015 at 12:01
Hi
I'm using STM32Cubef4 USB Host CDC library on STM32F429I-Discovery.
I have problem to connect a FTDI device.
The USB host process returnHOST_ABORT_STATE because the FTDI class is 0xFF (Vendor...
Posted on January 31, 2014 at 11:27Thanks for fast reply.I'm not using coocox ide, im using Eclipse + ARM GCCI add ''-lm'' to linker but nothing change.arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length...
Posted on January 31, 2014 at 10:34Hi,I have the same problem. When i compile, compiler show me this error:C:\TechKnow\STemWin_GUI_lib\STemWin_Library_V1.1.1\Libraries\STemWinLibrary522\Lib\libSTemWin522_CM4_GCC.a(WM_Motion.o): In function `_AimDest...