2016-04-28 4:06 AM
Hey community,
I am using StemWin 5.28 on the STM32f429 DISC1 board. I created a Windows with the GUIBuilder. This windows contains a button with the text ''start''. If I press the button something should happen. This is not the problem. If I press the button the function I implemented runs. But now I want to activate this button with an extern button to. I connected an extern button to an I/O-Pin. Reading the button is no problem. Is the button is pressed, the MCU recognize this. If I press the extern the button, the window should get the message that this button is pressed. But I have no idea how I should implement that. The documentation of emWin is not helpfull for me. Maybe someone can help me please? Thanks :)2016-04-28 5:49 AM
Okay I managed the problem.
I analysed the message which is send, when the button is released and build a similar one for the physical button. But now I have another problem. The physical buttons and the touch screen are controlled by a independent timer and an ISR. If a physical touch was detected a Message box appears in which the user has to press OK. But the timer for the touch screen doesn't trigger anymore. What can I do so that the timer trigger anyway? Thanks :)2016-04-28 10:38 AM
Hi fetzer.marcel, ,
Try to figure out inside the ''STM32F0 STMTouch library '' associated with user manual-Hannibal-
2016-05-09 5:36 AM
Hello,
i have to reactivate this thread again. I have still a problem with the command WM_SendMessage. The structure needs a hWinSrc but I dont know which value a I have to give this. I managed the problem by observing the message while debugging. So I build a similar message and it works. In my case I have to give hWinSrc the value 50. But now I reorganized the window by some new buttons. The old ones still exists. Now my message doesn't work anymore. Can I give hWinSrc a name as variable or something like this? Thanks :)