2015-06-05 11:27 AM
Hello,
Maybe a silly question but I have the latest CubeMX (4.8.0) and STM32F4 (1.6.0). I am able to see the STemWin directories and code under the CubeMX repository but I cannot find any way to generate a project including STemWin Library. My MCU is stm32F429. The LTDC peripheral is enabled. I cannot find any option in the CubeMX environment in order to enable the library. Is it possible to generate a project including StemWin or I have to do it manual ?Thanks in advance2015-06-09 4:21 AM
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-07-01 12:51 AM