cancel
Showing results for 
Search instead for 
Did you mean: 

STC3100, read to Control register is not returning the proper value

Suhas Kudale
Associate
Posted on March 24, 2017 at 09:12

Hi all. I need a help regarding I2C write operation on one of the register of STC3100. There are two configurable registers, one is 'Mode register' and other is 'Control register'.I noticed that writing to the Control register is not working. When I write a value on control register, lets say 0x12 or any value,and then whenever I try to read that register it gives value as 0x10 everytime. Could you explain why it is happening so?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Maarten Weyn
Associate
Posted on July 13, 2017 at 12:49

0x02 is a self clearing bit (see page 15 of the manual) so you will always read it as 0.