cancel
Showing results for 
Search instead for 
Did you mean: 

State of GPIO after Watchdog Reset

JBlackann
Associate III

Hello,

I am using a STM32F401CE and would like to use the independent watchdog to cause a reset if the device would lock up for some reason. I have an external chip which is being controlled via GPIO and SPI from the STM32F401. When a watchdog reset occurs, does the GPIO outputs all default to Off? Is there I could keep an I/O line high (SET) over a Watchdog reset? I would like to not reset the external device if a watchdog event occurred.

Thanks.

Josh

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Uwe Bonnes
Chief

Watchdog reset is like normal reset, setting all GPIO to default state. Only external pull cat set defined state.

View solution in original post

1 REPLY 1
Uwe Bonnes
Chief

Watchdog reset is like normal reset, setting all GPIO to default state. Only external pull cat set defined state.