2025-07-07 9:20 AM
Hi,
I am on stm32u585 IOT dev board for low power modes am using RTC wakeup the sleep and stop 1,2 and 3 are working fine but standby and shutdown is not working ? my code
void sleep(int mode, int seconds ) {
if (seconds <= 0) return;
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);
uint32_t wakeup_counter (uint32_t)(seconds 2048);
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, wakeup_counter, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0);
switch (mode) {
case 0: // Sleep
HAL_SuspendTick();
HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
HAL_ResumeTick();
break;
case 1: // Stop0
HAL_SuspendTick();
HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);
break;
case 2: // Stop1
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
break;
case 3: // Stop2
HAL_SuspendTick();
HAL_PWREx_EnterSTOP3Mode(PWR_STOPENTRY_WFI);
break;
case 4: // Standby
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG | PWR_FLAG_SBF);
HAL_PWR_EnterSTANDBYMode();
break;
case 5; // Shutdown/DeepSleep
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG | PWR_FLAG_SBF);
HAL_PWREx_EnterSHUTDOWNMode();
break;
default:
break;
}
}
void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *hrtc) {
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
SystemClock_Config();
HAL_ResumeTick();
}
2025-07-08 3:39 AM
Hello @shivss
The device cannot enter on standby and shutdown mode or cannot exit?
Please refer to the example below:
Note that The RTC remains active when the RTC clock source is LSE or LSI.
2025-07-08 6:01 AM - edited 2025-07-08 6:04 AM
Hi,
It is not exit from standby and shutdown modes. The example code is using Wakeup pin but want I need is wakeup with RTC .In RTC INIT checking for wakeup same as in example . This code is working for sleep,stop1,2 and 3 the RTC is working fine with these modes but not for standby or shutdown even UART messages are also not printing after standby or shutdown
static void MX_RTC_Init(void)
{
/* USER CODE BEGIN RTC_Init 0 */
uart_send("RTC start\r\n");
// Check if waking from Standby — if yes, skip full init
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SBF) != RESET)
{
uart_send(">> Woke from STANDBY\r\n");
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SBF); // Clear standby flag
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
}
/* USER CODE END RTC_Init 0 */
void sleep(int mode, int seconds ) {
if (seconds <= 0) return;
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);
uint32_t wakeup_counter (uint32_t)(seconds 2048);
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, wakeup_counter, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0);
switch (mode) {
case 0: // Sleep
HAL_SuspendTick();
HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
HAL_ResumeTick();
break;
case 1: // Stop0
HAL_SuspendTick();
HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);
break;
case 2: // Stop1
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
break;
case 3: // Stop2
HAL_SuspendTick();
HAL_PWREx_EnterSTOP3Mode(PWR_STOPENTRY_WFI);
break;
case 4: // Standby
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG | PWR_FLAG_SBF);
HAL_PWR_EnterSTANDBYMode();
break;
case 5; // Shutdown/DeepSleep
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG | PWR_FLAG_SBF);
HAL_PWREx_EnterSHUTDOWNMode();
break;
default:
break;
}
}
void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *hrtc) {
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
SystemClock_Config();
HAL_ResumeTick();
}
2025-07-08 12:55 PM
Hello @shivss
Could you please ensure that the RTC wake-up timer interrupt is properly configured by adding the following functions ? Once done, kindly let us know if the issue persists:
/* Enable WakeUp line functionality for the RTC ALARMA */
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN7_HIGH_3);
/* Enable the Autonomous Mode for the RTC */
__HAL_RCC_RTCAPB_CLKAM_ENABLE();
Best regards,
Haifa.