2018-05-14 2:29 AM
I'm hoping someone can provide a straight-forward answer as to how I can operate multiple stepper motors using stacked IHM06A1 boards. In example code, the STSpin220 class is initialised as
motor = new STSpin220(D2, D8, D7, D5, D10, D3, PWM_REF_PIN);
Is there a simple way of declaring two 'motors' in this way, perhaps with a small hardware mod?
Thanks
#stepper-motor #stspin220 #ihm06a1