cancel
Showing results for 
Search instead for 
Did you mean: 

ST Link Utility v3.4 ?

jamie23
Associate II
Posted on May 13, 2014 at 11:31

Hi All, I'm interested in the feature detailed in the v3.4 changelist which allows probe selection if multiple probes are connected, but the only version for download appears to be 3.3. Any clues as to the location of 3.4?

http://www.st.com/web/catalog/tools/FM147/SC1887/PF258168

''Version 3.4

New features

...

Added support of ST-LINK probe selection when more than one is connected to the

computer''

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/release_note/DM00034783.pdf

5 REPLIES 5
Posted on May 13, 2014 at 15:58

Seems to be missing, will push to moderation

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nickname306_O
Senior
Posted on May 13, 2014 at 17:53

Hi campbell.jamie,

STM32 ST-LINK Utility v 3.4 is still

under development. It

will be published on ST web site by end of this week.

I will let you know once available.

Best Regards,

Nouha

jamie23
Associate II
Posted on May 13, 2014 at 18:43

Great, thanks.

Just as a heads-up, will probe selection be supported from the CLI? If not, it's not going to solve my problem anyway. Hope this will be available.

Regards,

Jamie.

Nickname306_O
Senior
Posted on May 15, 2014 at 12:43

Hi Jamie,

Yes , it will be supported.

Best regards,

Nouha

jamie23
Associate II
Posted on May 21, 2014 at 11:25

Hi, is version 3.4 any closer to being released?

Thanks.