2015-08-24 06:34 PM
Can the program image generated by MDK be loaded/written directly into STM32F4
flash using ST-Link Utility, without using MDK to orchestrate the load by ST-Link Utility ?2015-08-24 09:12 PM
Yes, check the ''Create .HEX'' under the Output options, as this is the format the ST-LINK Utilities can process.