cancel
Showing results for 
Search instead for 
Did you mean: 

ST Link Utility direct load of STM32 flash without MDK

mkbrown32
Associate II
Posted on August 25, 2015 at 03:34

Can the program image generated by MDK be loaded/written directly into STM32F4

flash using ST-Link Utility, without using MDK to orchestrate the load

by ST-Link Utility ?

1 REPLY 1
Posted on August 25, 2015 at 06:12

Yes, check the ''Create .HEX'' under the Output options, as this is the format the ST-LINK Utilities can process.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..