cancel
Showing results for 
Search instead for 
Did you mean: 

ST link unable to connect STM32F205

PNova.2
Associate II

Hello
I swapped STM32F072RBT6 for STM32F205RCT6 on the board (I needed more RAM) and even though the cases are pin-compatible (LQFP64) ST llink v2 reports that it cannot connect to the target.
ST link works reliably on STM32F072RBT6.
I tried to connect via CUBE IDE debug and CUBE programmer - the result is the same.
Soldering checked.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
gbm
Principal

The cases are NOT pin-compatible. Note the VCAP pins - they must NOT be grounded but connected to external capacitors. Also, from my experience, fiddling with connect options may help (normal vs. under reset, etc.:

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

View solution in original post

3 REPLIES 3
gbm
Principal

The cases are NOT pin-compatible. Note the VCAP pins - they must NOT be grounded but connected to external capacitors. Also, from my experience, fiddling with connect options may help (normal vs. under reset, etc.:

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

Thanks
so I will have to use the same family because changes on the PCB are no longer possible.
Otherwise it would be easy - I would bypass the capacitors.

Look at L4 and L0 families - they should be pin-compatible with F0.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice