cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link_CLI.exe Can't Access Some Core Commands

souheil
Associate
Posted on April 28, 2015 at 01:37

Hello Sir,

I work on an evaluation board stm32f4 discovery, using ST-Link Utility v3.6 on Windows 8 with an usb connection. When I load an hex into memory, the command to run application fails with the message no target connected. Using the visual interface based on MFC and STLinkUSBDriver.dll, it works, but i need to do the work programatically. What  i have  to do to make the application running using ST-Link_CLI ? All  commands works except some Core Commands. Thanks a lot for help. 
1 REPLY 1
tarekbouchkati
Associate II
Posted on June 18, 2015 at 09:54

Hello Souheil,

Can you share with us the command sequence that generates the error.

Best Regards,

Ibn Ziyed