Skip to main content
LMI2
Senior III
October 26, 2017
Question

ST, don't use /** **/ for one line comments

  • October 26, 2017
  • 3 replies
  • 2211 views
Posted on October 26, 2017 at 22:43

Because IDE does not like nested comments. I am commenting several lines of example code but some idiot has put every other line an one line a /* */ comment.

Fix that software please.

Not like this:

 /* Insert a delay of display */
 HAL_Delay(2);
 }
 /* Clear the Background Layer */
 BSP_LCD_Clear(LCD_COLOR_BLACK);�?�?�?�?�?�?

//

    This topic has been closed for replies.

    3 replies

    S.Ma
    Principal
    October 27, 2017
    Posted on October 27, 2017 at 06:55

    Maybe call this a MISRA consequence more than ST's for compatibility with all users out there

    (for industrial or automotive, sometime the tools are kept the same for 10 years without upgrades)

    https://stackoverflow.com/questions/9538589/rationale-for-comment-rules-in-misra

     

    My workaround for this is 

    #if 0

    junked source code

    #endif

    AVI-crak
    Senior
    October 27, 2017
    Posted on October 27, 2017 at 09:11

    / * Used for compatibility with dinosaurs from 1998 * /

    Modern IDs often get malfunctioned in the code syntax highlighting module - due to stack overflow. There is a technical limit of 65k lines - below which the plug-in begins to suffer from amnesia. When the amnesia boundary falls / * neatly between several lines of comments * / - the synchronization is violated and the user sees a frank porridge. For example, the incorrect operation of conditional operators #if.

    Everything was fine while the projects were thin.

    Using // for comment, and /// for an important comment - solves the problem of amnesia.
    LMI2
    LMI2Author
    Senior III
    October 27, 2017
    Posted on October 27, 2017 at 15:59

     ,

     ,

    Interesting

    I wonder why Keil Ide is so upset of this when this problem has been there for years.

    I have to try this

    ♯ if 0

    junked source code

    ♯ endif

    Using // for comment, and /// for an important comment - solves the problem of amnesia.

    Yes but when the one with dementia is ST, what can you do.

    LM