2024-07-15 1:15 PM
We have a STM32H7 based device that we want to communicate with over serial using USB. We created the USB Composite driver using the sample code.
When we connect our device to Windows it shows up as a Serial Port (COM12).
When we connect it to MacOS it just shows up as a USB Composite device and I can't figure out how to get it to show up as a serial port.
How do we fix this?
2024-07-15 5:24 PM
Check the USB enumeration (all the descriptors the MCU will send). Use a USB debugger/analyzer. I assume, your descriptors (enumeration) is slightly wrong.
2024-07-16 6:34 AM
Thank you for the suggestions.
Would you be willing to give some guidance on exactly what I am looking for? If the descriptors are wrong, then why does it work just fine on Windows? Does that give us any clues as to what exactly might be wrong with the descriptors?
We took the values from the basic example.
2024-07-18 8:27 AM
I installed a usb analyzer tool on my Windows computer. Below are the items I was able to see. Can you identify what might be incorrect or missing for MacOS that Windows doesn't care about?
Device Descriptors:
Port: 1
Speed: Full Speed
Device address: 15
Open pipes: 3
Connection status: Device connected
Device Descriptor
USB version: 2.0
Device class: 0xef - Miscellaneous Device
Device subclass: 0x2 - ?
Device protocol: 0x1 - Interface Association
Control pipe max size: 64 bytes
Vendor ID: 0x483 (STMicroelectronics)
Product ID: 0x52a4 (Unknown)
Product version: 2.0
Manufacturer: HolleyTuningGroup
Product: HTG COMPOSITE DEVICE
Serial Number: 356739573532
Configurations: 1Configuration Descriptors:
descriptors[0] = "Configuration Descriptor"
bLength = 9
bDescriptorType = USB_CONFIGURATION_DESCRIPTOR_TYPE (2)
wTotalLength = 75
bNumInterfaces = 2
bConfigurationValue = 1
iConfiguration = 0
Reserved = 0
SupportsRemoteWakeup = 0
SelfPowered = 1
PoweredByBus = 1
MaxPower = 0x32 -> 100 mA
descriptors[1] = "Interface Association Descriptor"
bLength = 8
bDescriptorType = USB_INTERFACE_ASSOCIATION_DESCRIPTOR_TYPE (11)
bFirstInterface = 1
bInterfaceCount = 2
bFunctionClass = 2
bFunctionSubClass = 2
bFunctionProtocol = 1
iFunction = 0
descriptors[2] = "Interface Descriptor"
bLength = 9
bDescriptorType = USB_INTERFACE_DESCRIPTOR_TYPE (4)
bInterfaceNumber = 1
bAlternateSetting = 0
bNumEndpoints = 1
bInterfaceClass = UsbCommunication (2)
bInterfaceSubClass = 2
bInterfaceProtocol = 7
iInterface = 0
descriptors[3] = "Class-Specific Interface Descriptor"
bLength = 5
bDescriptorType = CS_INTERFACE (36)
bDescriptorSubtype = 0
comm_interface =
bcdCDC = 272
descriptors[4] = "Class-Specific Interface Descriptor"
bLength = 5
bDescriptorType = CS_INTERFACE (36)
bDescriptorSubtype = 1
comm_interface =
call_capatibilities =
controls =
UseClassInterface = 0
SelfControl = 0
Reserved = 0
bmCapatibilities = 0
bDataInterface = 00000010
descriptors[5] = "Class-Specific Interface Descriptor"
bLength = 4
bDescriptorType = CS_INTERFACE (36)
bDescriptorSubtype = 2
comm_interface =
abstract_control_capatibilities =
controls =
FeatureSupport = 0
LineStateSupport = 1
Send_Break_Support = 0
NotificationSupport = 0
Reserved = 0
bmCapatibilities = 00000010
descriptors[6] = "Class-Specific Interface Descriptor"
bLength = 5
bDescriptorType = CS_INTERFACE (36)
bDescriptorSubtype = 6
comm_interface =
bMasterInterface = 1
bSlaveInterface = { 2 }
descriptors[7] = "Endpoint Descriptor"
bLength = 7
bDescriptorType = USB_ENDPOINT_DESCRIPTOR_TYPE (5)
bEndpointAddress = 3
Reserved = 0
Direction = Input
type = Interrupt (3)
reserved = 0
wMaxPacketSize = 8
bInterval = 16
descriptors[8] = "Interface Descriptor"
bLength = 9
bDescriptorType = USB_INTERFACE_DESCRIPTOR_TYPE (4)
bInterfaceNumber = 2
bAlternateSetting = 0
bNumEndpoints = 2
bInterfaceClass = UsbCommData (10)
bInterfaceSubClass = 0
bInterfaceProtocol = 0
iInterface = 0
descriptors[9] = "Endpoint Descriptor"
bLength = 7
bDescriptorType = USB_ENDPOINT_DESCRIPTOR_TYPE (5)
bEndpointAddress = 2
Reserved = 0
Direction = Output
type = Bulk (2)
reserved = 0
wMaxPacketSize = 64
bInterval = 0
descriptors[10] = "Endpoint Descriptor"
bLength = 7
bDescriptorType = USB_ENDPOINT_DESCRIPTOR_TYPE (5)
bEndpointAddress = 2
Reserved = 0
Direction = Input
type = Bulk (2)
reserved = 0
wMaxPacketSize = 64
bInterval = 0
2024-07-18 8:29 AM
I am still getting used to this forum's method of posting. I posted a reply to the main post instead of to you. I don't know if that will give you a notification or not, so I am writing this reply directly to you.