2015-07-18 5:10 PM
Just wanted to give a heads up to this.
First of all, I am sorry if it was already referenced but I could not find anything when using the search tool.I have the V1.5.0 standard peripheral library package for F0 series. I also have V1.4.0.One thing I noticed is that the V1.5.0 is missing all the drivers info!There's nothing there as far as I am aware, when I got to ''Modules'' there is nothing there for them, when I searched for it further I had no success in finding the information. I downloaded again the package and as of now, July the 19th of 2015, the problem still persists.To note that in V1.4.0 there was also a problem with it, the info for the timer drivers was not present in the correct place, and was instead on the page before it, named ''STM32F0xx_StdPeriph_Driver''.I find that help file really useful and wanted to bring attention to this problem with hope it is fixed. I know most of that info can be found in the source files btw. #.chm-f0-spl-library-help-file2015-07-22 3:16 AM
Hi,
You are right;all the drivers info is missing.It is noted and will be fixed in coming release of the STM32F0 standard peripheral library.-Syrine