cancel
Showing results for 
Search instead for 
Did you mean: 

SPI2 clock

pinwu
Associate II
Posted on December 16, 2009 at 07:45

SPI2 clock

10 REPLIES 10
pinwu
Associate II
Posted on May 17, 2011 at 12:20

Hello,

I modified the evaluation board source codes to use SPI2 as a master, but I could get clock signal for PB13.

asterix
Associate II
Posted on May 17, 2011 at 12:20

Hi pinwu1,

PB13 (SPI2_CLK) is used in the Evaluation board from ST (MB525) to drive the TFT LCD and is working fine on my board, I suggest you to re-check your code for sure you have something missing in the initilisation. :)

Magigimix

pinwu
Associate II
Posted on May 17, 2011 at 12:20

I studied that part of source code. That clock for LCD is not generated by SPI internal clock. I simplified the code to initialize SPI registers and releated clocks only. I tested on this way, and found SPI1 working, but not SPI2.

For STM32F103RB chip, both SPI1 and SPI2 not working.

Thank You,

pinwu
Associate II
Posted on May 17, 2011 at 12:20

Quote:

On 27-12-2007 at 19:41, Anonymous wrote:

Hi pinwu1,

PB13 (SPI2_CLK) is used in the Evaluation board from ST (MB525) to drive the TFT LCD and is working fine on my board, I suggest you to re-check your code for sure you have something missing in the initilisation. :)

Magigimix

pinwu
Associate II
Posted on May 17, 2011 at 12:20

I posted my part of source code here.

void Set_System()

{

GPIO_InitTypeDef GPIO_InitStructure;

// if (mode == 1) { // DFU mode

// FLASH_Unlock();

// }

/* SYSCLK, HCLK, PCLK2 and PCLK1 configuration ------------*/

/* RCC system reset(for debug purpose) */

RCC_DeInit();

/* Enable HSE */

RCC_HSEConfig(RCC_HSE_ON);

/* Wait till HSE is ready */

HSEStartUpStatus = RCC_WaitForHSEStartUp();

if(HSEStartUpStatus == SUCCESS)

{

/* HCLK = SYSCLK */

RCC_HCLKConfig(RCC_SYSCLK_Div1);

/* PCLK2 = HCLK */

RCC_PCLK2Config(RCC_HCLK_Div1);

/* PCLK1 = HCLK/2 */

RCC_PCLK1Config(RCC_HCLK_Div2);

/* ADCCLK = PCLK2/6 */

RCC_ADCCLKConfig(RCC_PCLK2_Div6);

/* Flash 2 wait state */

FLASH_SetLatency(FLASH_Latency_2);

/* Enable Prefetch Buffer */

FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

/* PLLCLK = 8MHz * 9 = 72 MHz */

RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9);

/* Enable PLL */

RCC_PLLCmd(ENABLE);

/* Wait till PLL is ready */

while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)

{

}

/* Select PLL as system clock source */

RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

/* Wait till PLL is used as system clock source */

while(RCC_GetSYSCLKSource() != 0x08)

{

}

/* USBCLK = PLLCLK / 1.5 */

RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5);

/* Enable USB clock */

RCC_APB1PeriphClockCmd(RCC_APB1Periph_USB, ENABLE);

}

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB |RCC_APB2Periph_GPIOC

| RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO, ENABLE);

USB_Cable_Config (DISABLE);

SPI_FLASH_Init();

USB_Cable_Config (ENABLE);

}

int main(void)

{

#ifdef DEBUG

debug();

#endif

Set_System();

while (1)

{

SPI_FLASH_ReadID(); // Test Only

}

}

void SPI_FLASH_Init(void)

{

SPI_InitTypeDef SPI_InitStructure;

GPIO_InitTypeDef GPIO_InitStructure;

/* Enable SPI1 and GPIOA clocks */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1 | RCC_APB2Periph_GPIOA, ENABLE);

// RCC_APB2PeriphClockCmd(RCC_APB1Periph_SPI2 | RCC_APB2Periph_GPIOB, ENABLE);

/* Configure SPI1 pins: NSS, SCK, MISO and MOSI */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;

// GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_Init(GPIOA, &GPIO_InitStructure);

// GPIO_Init(GPIOB, &GPIO_InitStructure);

/* Configure PA.4 as Output push-pull, used as Flash Chip select */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

// GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_Init(GPIOA, &GPIO_InitStructure);

// GPIO_Init(GPIOB, &GPIO_InitStructure);

/* Deselect the FLASH: Chip Select high */

SPI_FLASH_CS_HIGH();

/* SPI1 configuration */

SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;

SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4;

SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_InitStructure.SPI_CRCPolynomial = 7;

SPI_Init(SPI1, &SPI_InitStructure);

// SPI_Init(SPI2, &SPI_InitStructure);

/* Enable SPI1 */

SPI_Cmd(SPI1, ENABLE);

// SPI_Cmd(SPI2, ENABLE);

}

In spi_flash.h,

/* Exported macro ---------*/

/* Select SPI FLASH: ChipSelect pin low */

#define SPI_FLASH_CS_LOW() GPIO_ResetBits(GPIOA, GPIO_Pin_4)

// #define SPI_FLASH_CS_LOW() GPIO_ResetBits(GPIOB, GPIO_Pin_12)

/* Deselect SPI FLASH: ChipSelect pin high */

#define SPI_FLASH_CS_HIGH() GPIO_SetBits(GPIOA, GPIO_Pin_4)

// #define SPI_FLASH_CS_HIGH() GPIO_SetBits(GPIOB, GPIO_Pin_12)

[ This message was edited by: pinwu1 on 28-12-2007 00:22 ]

asterix
Associate II
Posted on May 17, 2011 at 12:20

Dear pinwu1,

I think that you mising part is in line :

/* Enable SPI1 and GPIOA clocks */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1 | RCC_APB2Periph_GPIOA, ENABLE);

// RCC_APB2PeriphClockCmd(RCC_APB1Periph_SPI2 | RCC_APB2Periph_GPIOB, ENABLE);

SPI2 is connected in APB1 and not like SPI1 which is connected to APB2 with all GPIOs.

So the right code to enbale SPI2 is something like :

/* Enable SPI2 and GPIOB clocks */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

Tell me if it is working well now ;) Magigimix ;)

ivan1
Associate II
Posted on May 17, 2011 at 12:20

My project has also this problem. The clk of SPI2 does not work at all, but there is signal on MOSI pin.

Already set like this RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

Quote:

On 28-12-2007 at 15:48, Anonymous wrote:

Dear pinwu1,

I think that you mising part is in line :

/* Enable SPI1 and GPIOA clocks */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1 | RCC_APB2Periph_GPIOA, ENABLE);

// RCC_APB2PeriphClockCmd(RCC_APB1Periph_SPI2 | RCC_APB2Periph_GPIOB, ENABLE);

SPI2 is connected in APB1 and not like SPI1 which is connected to APB2 with all GPIOs.

So the right code to enbale SPI2 is something like :

/* Enable SPI2 and GPIOB clocks */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

Tell me if it is working well now ;) Magigimix ;)

pinwu
Associate II
Posted on May 17, 2011 at 12:20

Dear Magigimix,

Thank you for your correction. It does still not work for SPI2 with this correction. Is there something wrong?

PinWu

pinwu
Associate II
Posted on May 17, 2011 at 12:20

For the evaluation borad, both SPI1 and SPI2 are working. I found that SPI_FLASH_SendByte was hard-coded for SPI1.

Thank You Magigimix